AXIS#.MOTOR​.BRAKEPOWERSAVING

Description

This parameter can be used to disable power saving brake operation. If disabled, only full voltage will be used to control the brake.

When power saving mode is enabled, full voltage is used to initiate release of brake. After waiting AXIS#.MOTOR.TBRAKERLS milliseconds for brake to mechanically release, an additional delay of AXIS#.MOTOR​.BRAKEPOWERDELAY milliseconds waits for brake to electrically stabilize before voltage is reduced to AXIS#.MOTOR​.BRAKEPOWERLOW.

Value Description
0 Power saving mode disabled
1 Power saving mode enabled

Context

For more information see Brake and Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

1

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.BRAKEPOWERSAVING

500bh

26h

Unsigned8

-

-

Read/Write

No

AXIS2.MOTOR.BRAKEPOWERSAVING

510bh

26h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.BRAKEPOWERSAVING

6240

1860

Unsigned8

Read Only

-

AXIS2.MOTOR.BRAKEPOWERSAVING

71776

1186

Unsigned8

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.BRAKEPOWERSAVING

6240

Unsigned8

Read Only

-